HC12: Accesssing external RAM using CS1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HC12: Accesssing external RAM using CS1

Jump to solution
3,516 Views
NZ_Design
Contributor I

I are new to code warrier and are trying to setup the ability to access external RAM on the address bus.

 

I are using the softec HCS12x starter kit.

 

I have set an variable in my code

 

#pragma DATA_SEG __DPAGE_SEG Bat_RAM

 char cExt_RAM;

#pragma DATA_SEG DEFAULT

 

I are setting cExt_RAM = 0x47.

 

And then trying to read it and send it back out the serial port (should get ‘G’ on my hyperterminal).

 

Works if I initialize it in internal ram.

 

In my startup code I have set Bat_RAM

 

SEGMENTS              /* paged RAM */

             BatteryRAM      = READ_WRITE    0x200000 TO 0x20FFFF;

END

 

PLACEMENT

             Bat_RAM              INTO  BatteryRAM;

END

 

In the map file cExt_RAM is mapped to 0x200000

 

This sould mean that it is mapped to CS1.

 

 

In my startup code I have set the device up as follows.

 MODE = 0xA0;        // MODC = 1, MODB = 0, MODA = 1 (Normal Expanded Mode)

 

 ECLKCTL = 0x43;                                // NECLK = 0 (Enabled)

                     // NECLKX2 = 1 (Disabled)

                     // EDIV = 3 (Bus clock div 4)

        

           EBICTL0 = 0x34;     // ITHRS = 0 (5v Logic levels).

                              // HDBE = 1 (16b data bus enabled

                              // Enable Address lines ADDR0:19 + /UDS

           

           EBICTL1 = 0x07;     // EWAITE = 0 (External wait Enabled is disabled)

                              // External Access stretch set to max of 8 cycles.

                              //    alter once working.

           

           MMCCTL0 = 0x0F;     // CS0:3 = 1 (Enabled)

           MMCCTL1 = 0x05;     // EROMON = 1, ROMHM = 0, ROMON = 1

           CLKSEL &= 0x7F;     // Ensure PLL unsellected

           for (i=0; i < 800; i++);

           SYNR = 39;          // 40 Mhz Bus clock

           for (i=0; i < 800; i++);

           REFDV = 15;         // 40 Mhz Bus clock

           for (i=0; i < 800; i++);

 

 while (CRGFLG & 0x08 == 0x08);        

 CLKSEL = 0x80;

           for (i=0; i < 800; i++);

 

I are experanced with the standard HCS12 but new to the S12x.

 

As far as I can tell the CS should work.

 

If I scope CS1 it doesn’t change state. Also the ECLK is not being stretched for the data read/write.

 

Can you please point me in the right direction.

 

Regards,

 

Daniel Rogers

Message Edited by CrasyCat on 2007-04-13 02:21 PM

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,167 Views
CompilerGuru
NXP Employee
NXP Employee
Use
#pragma DATA_SEG __GPAGE_SEG Bat_RAM

DPAGE is for a HC12 A4, not for a HCS12X.

Also use the 'G suffix for the global addresses in the prm file.
E.g.:

BatteryRAM = READ_WRITE 0x200000'G TO 0x20FFFF'G;

(also use 'G only for this one, keep the logical ones for code)

Also either make BatteryRAM NO_INIT, or add a option -D__FAR_DATA to your compiler options (by default far data is not initialized).


Daniel

View solution in original post

0 Kudos
Reply
2 Replies
2,168 Views
NZ_Design
Contributor I
Thanks I are underway and working.
 
Daniel
0 Kudos
Reply
2,168 Views
CompilerGuru
NXP Employee
NXP Employee
Use
#pragma DATA_SEG __GPAGE_SEG Bat_RAM

DPAGE is for a HC12 A4, not for a HCS12X.

Also use the 'G suffix for the global addresses in the prm file.
E.g.:

BatteryRAM = READ_WRITE 0x200000'G TO 0x20FFFF'G;

(also use 'G only for this one, keep the logical ones for code)

Also either make BatteryRAM NO_INIT, or add a option -D__FAR_DATA to your compiler options (by default far data is not initialized).


Daniel
0 Kudos
Reply