HC05 to HCS08 transition help

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HC05 to HCS08 transition help

1,036件の閲覧回数
saravanananbazh
Contributor II

I am currently working on a project that requires transition of old HC05 chip to HCS08 chip.

I get the below error when U compile the code (Byte craft C6808 compiler)

****2\S08_Reg.h 4:2:Unexpected error (1) in object file R  0052 #pragma regac # SEC return # enum registercc # registercc

****2\S08_Reg.h 4:2:Unexpected error (1) in object file T  0054 #pragma regac # SEC return # enum registercc # registercc

****22\S08_Reg.h 4:2:Unexpected error (1) in object file p  0070 #pragma regac # SEC return # enum registercc # registercc # enum auto bits registercc # return SEC }

****22\S08_Reg.h 4:2:Unexpected error (1) in object file r  0072 #pragma regac # SEC return # enum registercc # registercc # enum auto bits registercc # return SEC }

****2\S08_Reg.h 4:2:Unexpected error (1) in object file a  0061 #pragma regac # SEC return # enum registercc # registercc # enum auto bits registercc # return SEC }

****2\S08_Reg.h 4:2:Unexpected error (1) in object file g  0067 #pragma regac # SEC return # enum registercc # registercc # enum auto bits registercc # return SEC }

****2\S08_Reg.h 4:2:Unexpected error (1) in object file m  006D #pragma regac # SEC return # enum registercc # registercc # enum auto bits registercc # return SEC }

 

please help me resolve this... S08_reg.h is a header file

 

Thanks

torres

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

951件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Saravanan Anbazhagan,

Could you tell us which CodeWarrior version and S08 MCU are you using?

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 件の賞賛
返信