GNU Tools for ColdFire

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GNU Tools for ColdFire

3,350件の閲覧回数
BTaylor
Contributor III

Does CodeWarrior for MCUs (v10.6) support the use of the gnu tools (gcc, ld, etc) for building projects for Coldfire processors?

ラベル(1)
タグ(3)
0 件の賞賛
返信
3 返答(返信)

2,748件の閲覧回数
BlackNight
NXP Employee
NXP Employee

It is Eclipse, it it does not prevent it to use any Eclipse tools (including GNU for ColdFire). CW comes with its own (proprietary, non-GNU) compiler for bare board targets, but it already includes GNU (Codesourcery) for Linux.

2,748件の閲覧回数
BTaylor
Contributor III

Thank you for your prompt and helpful response.

So that I am sure I understand you...CodeWarrior provides, for bare board ColdFire targets, a proprietary, non-gnu compiler, but does not constrain the eclipse IDE in any way as to inhibit a developer from integrating and using the gnu toolchain for these targets. Correct?

Followup...Does CodeWarrior provides the gnu toolchain for bare board Kinetis targets? If so, are there any plans for an upcoming CodeWarrior release to provide the gnu toolchain in the same manner for bare board Coldfire targets?

Thank you.

0 件の賞賛
返信

2,748件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Yes, CW includes a non-GNU compiler for bar board (or RTOS) ColdFire targets, and you can integrate any toolchain you want into Eclipse.

And yes, CodeWarrior does include the GNU toolchain for bare board (and RTOS) Kinetis targets for more than two years. There are no plans for Linux targets (as Kinetis devices are too small). And there is the Kinetis Design Studio too (recently announced, www.freescale.com/kds) which includes the GNU toolchain for ARM.

0 件の賞賛
返信