Function does not get the correct passed argunment

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Function does not get the correct passed argunment

2,226 次查看
HYIU
Contributor I

Hi expert,

 

I have a simple program running in HCS08AC128 simulation mode.  I found that the argunment passed to a function cannot be correctly received by the function.  In main, I call this function SD_CLKDelay (8).  This is the function:

 

 

  void SD_CLKDelay (byte Frames)
  {
      while (Frames--)
          SPI_Send_byte (0xFF);
  }

 

 

Now, if I single step [F5] into this function, the variable Frames should show 8, but instead it shows 0x21 in the variable window.  Here is assembly for main calling:

 

 

  0014 a608   [2]  LDA #8

  0016 cd0000 [6]  JSR SD_CLKDelay

 

 

but the logic of the function is still correct when looking at the assembly

 

 

 

  0000 2008   [3]  BRA LA ;abs = 000a

  0002 L2:

  0002 aeff   [2]  LDX #-1

  0004 8c     [1]  CLRH

  0005 87     [2]  PSHA

  0006 cd0000 [6]  JSR SPI_Send_byte

  0009 86     [3]  PULA

  000a LA:

  000a 97     [1]  TAX

  000b 4a     [1]  DECA

  000c 5d     [1]  TSTX

  000d 26f3   [3]  BNE L2 ;abs = 0002

 

 

but when I single step and goes to inside the SPI_Send_byte() function, the variable is wrong and the actual behavior is also wrong.  Here is what happen in the assembly:

 

 

  0000 87       [2]             PSHA 
  0001          L1:    
  0001 0b00fd   [5]             BRCLR 5,_SPI1S,L1 ;abs = 0001
  0004 b600     [3]             LDA   _SPI1S
  0006 95       [2]             TSX  
  0007 f6       [3]             LDA   ,X
  0008 b700     [3]             STA   _SPI1D
  000a          LA:    
  000a 0f00fd   [5]             BRCLR 7,_SPI1S,LA ;abs = 000a
  000d b600     [3]             LDA   _SPI1D
  000f 8a       [3]             PULH 
  0010 81       [6]             RTS  

Now it is obvious that the argunment 0xFF passed to the function is lost.

 

 

So there are two problems:

1. Why the compiler compile the code incorrectly?

2. Why the debugger simulator showing the incorrect variable values?

 

 

I am using the latest CodeWarrior Development Studio just downloaded from Freescale, and using all the default build configuration.

 

 

BR - Henry

 

标签 (1)
标记 (1)
0 项奖励
回复
4 回复数

1,720 次查看
CompilerGuru
NXP Employee
NXP Employee

Do you have any compiler warnings about implicitly declared functions? Take those very seriously, if the implied type does not 100% match the actual type then such argument passing bugs are happening. And the implicitly deduced types rarely match the declared ones, ....

 

Daniel

 

 

0 项奖励
回复

1,720 次查看
HYIU
Contributor I

Hi Daniel,

 

Thanks for your answer.  Yes, the "implicitly declared function" warning was there.  After I put in function prototypes, then the problem goes away.  I was wondering if it is possible to make this into an error instead of warning?  Mismatch function prototype should be considered a very serious mistake and should be regarded as error to make sure the programmer fix it before going on.

 

The other problem should be just regarded as the debugger watch window problem which should not affect the normal operation of the code.

 

 

0 项奖励
回复

1,720 次查看
Lundin
Senior Contributor IV

I think this should be an error as well. If I remember correctly, declaring functions without a prototype is considered an obsolete part of the C language by the standard committee, and they will likely remove it from the language should there ever be a new standard released.

 

 

0 项奖励
回复

1,720 次查看
Emac
Contributor III

You can set the C compiler options to regard "implicitly declared function" warnings as an error instead:

 

option -Wpd in the C compiler options.

 

Also available in the drop down menu Edit>XXXX Settings>Compiler for HCXX>Messages>Error for implicit parameter declaration

 

 (default is unclicked and disabled)

0 项奖励
回复