Full license CodeWarrior

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Full license CodeWarrior

Jump to solution
4,773 Views
baonguyen
Contributor I
Dear everybody

I have used CodeWarrior 5.1 (for HC08 and HCS08) anh when I compile a project having more 32 files. CW 5.1 has error:" This IDE is not licensed for full functionality, so there is a limit of 32 files per target"

What do I do to get full license ? And how to update CW (for HC08 and HCS08) for supporting other MCU like: GR, AZ ...

Thank you very much
Best regards
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,147 Views
CrasyCat
Specialist III

Hello

This message usually comes when you are using a special edition of CodeWarrior for HC08.

In order to remove this limitation you have to upgrade to at least a 32K upgrade license.

Please check following URL for detail show to purchase teh poroduct.

http://www.freescale.com/webapp/sps/site/homepage.jsp?nodeId=01098400786959705928692

Crasycat

View solution in original post

0 Kudos
Reply
2 Replies
2,147 Views
RockyRoad
Contributor III
CodeWarrior 5.1 for HC(S)08 and RS08 does support the AZ and GR. What specific MCU are you looking for?  You could also see the following document for the complete list of the MCU's supported:
 
 
- Rocky

Message Edited by RockyRoad on 2006-06-16 02:31 PM

2,148 Views
CrasyCat
Specialist III

Hello

This message usually comes when you are using a special edition of CodeWarrior for HC08.

In order to remove this limitation you have to upgrade to at least a 32K upgrade license.

Please check following URL for detail show to purchase teh poroduct.

http://www.freescale.com/webapp/sps/site/homepage.jsp?nodeId=01098400786959705928692

Crasycat

0 Kudos
Reply