Full license CodeWarrior

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Full license CodeWarrior

ソリューションへジャンプ
4,738件の閲覧回数
baonguyen
Contributor I
Dear everybody

I have used CodeWarrior 5.1 (for HC08 and HCS08) anh when I compile a project having more 32 files. CW 5.1 has error:" This IDE is not licensed for full functionality, so there is a limit of 32 files per target"

What do I do to get full license ? And how to update CW (for HC08 and HCS08) for supporting other MCU like: GR, AZ ...

Thank you very much
Best regards
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,112件の閲覧回数
CrasyCat
Specialist III

Hello

This message usually comes when you are using a special edition of CodeWarrior for HC08.

In order to remove this limitation you have to upgrade to at least a 32K upgrade license.

Please check following URL for detail show to purchase teh poroduct.

http://www.freescale.com/webapp/sps/site/homepage.jsp?nodeId=01098400786959705928692

Crasycat

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,112件の閲覧回数
RockyRoad
Contributor III
CodeWarrior 5.1 for HC(S)08 and RS08 does support the AZ and GR. What specific MCU are you looking for?  You could also see the following document for the complete list of the MCU's supported:
 
 
- Rocky

Message Edited by RockyRoad on 2006-06-16 02:31 PM

2,113件の閲覧回数
CrasyCat
Specialist III

Hello

This message usually comes when you are using a special edition of CodeWarrior for HC08.

In order to remove this limitation you have to upgrade to at least a 32K upgrade license.

Please check following URL for detail show to purchase teh poroduct.

http://www.freescale.com/webapp/sps/site/homepage.jsp?nodeId=01098400786959705928692

Crasycat

0 件の賞賛
返信