Full Scale Sim. on a S19 file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Full Scale Sim. on a S19 file

ソリューションへジャンプ
1,693件の閲覧回数
BobMac
Contributor I

Hi Everybody;

 How can we run a full scale simulation on a S19 file?

We would like to load a s19 file and run the simulator on it. Is this possible?

I know we used to be able to do this with our PEmicro tools and I suspect there is a 

way to do this in our Code Warrior tools.

 

Regards, Bob

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
966件の閲覧回数
stanish
NXP Employee
NXP Employee

Hello BobMac,

 

Yes, you can run simulation on a S19 file using CodeWarrior debugger.

1) run the debugger in simulation mode (menu "Component" -> "Set Connection..." ->" Connection: Full Chip Simulation")

2) select appropriate MCU derivative in the debugger

3) Load s19 file (menu "File" -> "Load Application..." -> select "Motorola S-Record..." as a File Type), uncheck option "Run after successful load", select your S19 file and press button "Load Code.

 

In the assembly window you should see .S19 file code.

 

Stanish

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
967件の閲覧回数
stanish
NXP Employee
NXP Employee

Hello BobMac,

 

Yes, you can run simulation on a S19 file using CodeWarrior debugger.

1) run the debugger in simulation mode (menu "Component" -> "Set Connection..." ->" Connection: Full Chip Simulation")

2) select appropriate MCU derivative in the debugger

3) Load s19 file (menu "File" -> "Load Application..." -> select "Motorola S-Record..." as a File Type), uncheck option "Run after successful load", select your S19 file and press button "Load Code.

 

In the assembly window you should see .S19 file code.

 

Stanish

 

0 件の賞賛
返信