Flexray Code Samples?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flexray Code Samples?

ソリューションへジャンプ
4,998件の閲覧回数
brian_s
Contributor I
Hi, I am currently starting a college project using the HCS 12 to setup a simple flexray network and CAN gateway. I am not sure as yet what version of code warrior I will need to get to cover the requirements of my project. Does anybody have any sample flexray code that I could use to get a rough idea of the program size for flexray?

Thanks
Brian
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,847件の閲覧回数
trytohelp
NXP Employee
NXP Employee
Hi,
 
The last version of HC12 is CodeWarrior for HC12 V4.6.
You can download it form our web site.
The Special edition license is installed by default.
If you need another version of the license please contact your local distributor.
You can have several versions installed on the same PC.
There is only one restriction: install them on separate folder.
 
For the Flexray, please refer to the web site
http://www.freescale.com/flexray
The Can driver is available with Processor Expert. However it's an advanced bean so available in pro version.
 
For details please refer to the buyer's guide
 
Pascal

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,847件の閲覧回数
Alban
Senior Contributor II
Hello,
 
Flexray sample code may be available by entering a Service Request to Freescale.
As far as I know it is a licensed protocol only authorized for use in Automotive yet.
 
Cheers,
Alban.
2,848件の閲覧回数
trytohelp
NXP Employee
NXP Employee
Hi,
 
The last version of HC12 is CodeWarrior for HC12 V4.6.
You can download it form our web site.
The Special edition license is installed by default.
If you need another version of the license please contact your local distributor.
You can have several versions installed on the same PC.
There is only one restriction: install them on separate folder.
 
For the Flexray, please refer to the web site
http://www.freescale.com/flexray
The Can driver is available with Processor Expert. However it's an advanced bean so available in pro version.
 
For details please refer to the buyer's guide
 
Pascal
0 件の賞賛
返信