Flexray Code Samples?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flexray Code Samples?

Jump to solution
5,008 Views
brian_s
Contributor I
Hi, I am currently starting a college project using the HCS 12 to setup a simple flexray network and CAN gateway. I am not sure as yet what version of code warrior I will need to get to cover the requirements of my project. Does anybody have any sample flexray code that I could use to get a rough idea of the program size for flexray?

Thanks
Brian
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,857 Views
trytohelp
NXP Employee
NXP Employee
Hi,
 
The last version of HC12 is CodeWarrior for HC12 V4.6.
You can download it form our web site.
The Special edition license is installed by default.
If you need another version of the license please contact your local distributor.
You can have several versions installed on the same PC.
There is only one restriction: install them on separate folder.
 
For the Flexray, please refer to the web site
http://www.freescale.com/flexray
The Can driver is available with Processor Expert. However it's an advanced bean so available in pro version.
 
For details please refer to the buyer's guide
 
Pascal

View solution in original post

0 Kudos
Reply
2 Replies
2,857 Views
Alban
Senior Contributor II
Hello,
 
Flexray sample code may be available by entering a Service Request to Freescale.
As far as I know it is a licensed protocol only authorized for use in Automotive yet.
 
Cheers,
Alban.
2,858 Views
trytohelp
NXP Employee
NXP Employee
Hi,
 
The last version of HC12 is CodeWarrior for HC12 V4.6.
You can download it form our web site.
The Special edition license is installed by default.
If you need another version of the license please contact your local distributor.
You can have several versions installed on the same PC.
There is only one restriction: install them on separate folder.
 
For the Flexray, please refer to the web site
http://www.freescale.com/flexray
The Can driver is available with Processor Expert. However it's an advanced bean so available in pro version.
 
For details please refer to the buyer's guide
 
Pascal
0 Kudos
Reply