Flash Programming fails

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Flash Programming fails

跳至解决方案
2,610 次查看
carrieowen
Contributor I

I am using CodeWarrior 10.6.4 with a P&E USB-ML-UNIVERSAL cable to connect to a Kinetis K60DN512VLL10.  Flash programming and debugging fail.  I have captured a diagnostic zip file.  I was using this on a different computer just fine, but I upgraded my computer and now the setup doesn't work.

Original Attachment has been moved to: 201601140924_DiagnosticInfo.zip

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,423 次查看
trytohelp
NXP Employee
NXP Employee

If a sample project is not working, the problem could be linked to the Multilink or to the Board.

Does the 2 lights (blue and orange) on Multilink are lighted ?

To simplify I can say the blue is for the connection between PC and Multilink and orange for connection between the multilink and board.

Under Windows Device Manager the Mulilink 2.0 should be displayed

pastedImage_0.png

Multilink is a P&E interface.

There are some FAQs on P&E web site.

Please have a look to:

    P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Development T...

    P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Development Tools...

Regards


Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,422 次查看
trytohelp
NXP Employee
NXP Employee

Hi Carrie,

This is my configuration:

    Win 7 64 bit

    CW for MCU V10.6.4 + Updates 5 & 6

    TWR-K60D100M (Based on K60DN512)

    Multilink Universal Rev B

With this configuration I've created an example with the project Wizard.

After to have build the project I can launch the debug session for Ram and Flash targets without problem.

Using the Flash file to Target , it's working fine too.

Can you try to create a sample project with the project Wizard ?

Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,422 次查看
carrieowen
Contributor I

I have created a sample project but get the same errors when programming or debugging.

-Carrie

0 项奖励
回复
2,424 次查看
trytohelp
NXP Employee
NXP Employee

If a sample project is not working, the problem could be linked to the Multilink or to the Board.

Does the 2 lights (blue and orange) on Multilink are lighted ?

To simplify I can say the blue is for the connection between PC and Multilink and orange for connection between the multilink and board.

Under Windows Device Manager the Mulilink 2.0 should be displayed

pastedImage_0.png

Multilink is a P&E interface.

There are some FAQs on P&E web site.

Please have a look to:

    P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Development T...

    P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Development Tools...

Regards


Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复