Flash Programmer for S12X

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash Programmer for S12X

3,695件の閲覧回数
Pogo
Contributor III

Hi all,

Does anyone know where can I get flash programmer for S12X? I'm using CodeWarrior 5.0, but it doesn't have flash programmer. I need flash programmer to write my firmware to MCU without opening project on CodeWarrior. Thanks a lot.

 

 

Pogo Lin

ラベル(1)
タグ(1)
0 件の賞賛
返信
6 返答(返信)

3,239件の閲覧回数
vishaka_maithil
Contributor I

Are you looking for Flash programming routines??????

0 件の賞賛
返信

3,239件の閲覧回数
Pogo
Contributor III

Yes, I need Flash Programmer. I found one document that explain how Freescale has integrated a powerful Flash Programmer into the CodeWarrior IDE. But I can't find this feature in my CodeWarrior ( version is 5.0 special edition).  Do you have any information about it?

0 件の賞賛
返信

3,239件の閲覧回数
kef
Specialist I

It is still not clear what do you need. Certainly CW comes with builtin debugger/programmer software. Are you going to flash binary file to your MCU? Ten you can start debugger <CW root folder>/prog/hiwave.exe

0 件の賞賛
返信

3,239件の閲覧回数
Pogo
Contributor III

Hi Kef,

I just want a standalone flash programmer to write my program into MCU. I need to program the MCU on the production line. I don't want to use CW's debug feature to program it. I want to integrate the standalone flash program to my production line.

 

Thanks a lot.

 

 

Regards,

Pogo

0 件の賞賛
返信

3,239件の閲覧回数
kef
Specialist I

Check www.pemicro.com 

Cyclone is certainly true standalone programmer. If you mean standalone programmer software, then it's PROG12z, which works with both Cyclone and Multilink.

0 件の賞賛
返信

3,239件の閲覧回数
J2MEJediMaster
Specialist I

I just looked at the CodeWarrior for HCS12(X) product matrix, and the Special Edition does support flash programming. You build your program for flash memory, hit debug, and CodeWarrior downloads and stores the program into flash automatically.

 

---Tom

0 件の賞賛
返信