Flash Programmer for S12X

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash Programmer for S12X

2,595 Views
Pogo
Contributor III

Hi all,

Does anyone know where can I get flash programmer for S12X? I'm using CodeWarrior 5.0, but it doesn't have flash programmer. I need flash programmer to write my firmware to MCU without opening project on CodeWarrior. Thanks a lot.

 

 

Pogo Lin

Labels (1)
Tags (1)
0 Kudos
Reply
6 Replies

2,139 Views
vishaka_maithil
Contributor I

Are you looking for Flash programming routines??????

0 Kudos
Reply

2,139 Views
Pogo
Contributor III

Yes, I need Flash Programmer. I found one document that explain how Freescale has integrated a powerful Flash Programmer into the CodeWarrior IDE. But I can't find this feature in my CodeWarrior ( version is 5.0 special edition).  Do you have any information about it?

0 Kudos
Reply

2,139 Views
kef
Specialist I

It is still not clear what do you need. Certainly CW comes with builtin debugger/programmer software. Are you going to flash binary file to your MCU? Ten you can start debugger <CW root folder>/prog/hiwave.exe

0 Kudos
Reply

2,139 Views
Pogo
Contributor III

Hi Kef,

I just want a standalone flash programmer to write my program into MCU. I need to program the MCU on the production line. I don't want to use CW's debug feature to program it. I want to integrate the standalone flash program to my production line.

 

Thanks a lot.

 

 

Regards,

Pogo

0 Kudos
Reply

2,139 Views
kef
Specialist I

Check www.pemicro.com 

Cyclone is certainly true standalone programmer. If you mean standalone programmer software, then it's PROG12z, which works with both Cyclone and Multilink.

0 Kudos
Reply

2,139 Views
J2MEJediMaster
Specialist I

I just looked at the CodeWarrior for HCS12(X) product matrix, and the Special Edition does support flash programming. You build your program for flash memory, hit debug, and CodeWarrior downloads and stores the program into flash automatically.

 

---Tom

0 Kudos
Reply