File limit for CW for HC08 microcontrollers V6.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

File limit for CW for HC08 microcontrollers V6.0

5,966件の閲覧回数
Nouchi
Senior Contributor II
Hello,

This document makes me confused about file limit, It doesn't talk about that.
Because I tried to add severals  files and  CW told me : 
" Project Error : 202049  This IDE is not licensed for full functionality, etc.........".
http://www.freescale.com/files/soft_dev_tools/doc/fact_sheet/CWS-H08-FS.pdf

Is it a documentation problem, or I need to register to have SE full functionality?


Emmanuel



Message Edited by BugMan on 2007-07-11 05:21 PM

Added MCU type to subject line


Message Edited by J2MEJediMaster on 2007-07-12 10:12 AM
ラベル(1)
タグ(1)
0 件の賞賛
返信
6 返答(返信)

3,139件の閲覧回数
BlackNight
NXP Employee
NXP Employee
Hello,
I could imagine that the error message you describe comes if you have not following key in your license file: Win32_CWIDE_Unlimited.
If you have only the 'limited' (and not the limited) key, then the IDE has a limit around 32 files and does not allow you to create sub projects. From my special edition key I do have above unlimited key in the license.dat file. Could you check if you have it it too?

Erich
0 件の賞賛
返信

3,139件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
In the license.dat automatically installed I have the Win32_CWIDE_Limited.
I did not register or do anything else.

Daniel

0 件の賞賛
返信

3,139件の閲覧回数
Nouchi
Senior Contributor II
Hi,

I have Win32_CWIDE_Limited too, but the compartive table doen't mention that.
This CW SE increased C code size (16k -> 32K), but the file limit is the same.
If you use Processor Expert,  the  limiot is quickly reached :smileysad:



Emmanuel
0 件の賞賛
返信

3,139件の閲覧回数
stanish
NXP Employee
NXP Employee
32 files per project limitation was removed with V6.0, but the license file was not updated. The new Special Edition license file (including feature Win32_CWIDE_Unlimited) can be downloaded from the CW for MCU V6.0 WEB page.

http://www.freescale.com/files/soft_dev_tools/doc/support_info/SELicense_CWMCUv60.dat
0 件の賞賛
返信

3,139件の閲覧回数
mke_et
Contributor IV
I've stayed with CW3.x for my 9S12 and HC08 projects because I was given one of those 'special' licenses for my 9S12 project that allowed unlimited files. I write in assembly so I didn't need the full feature license.

Keeping everything on CW3.x was only for consistancy so that I could have the same development system for everything. I didn't upgrade CW because I didn't want to have to get a new license for my 9S12 projects, which were getting quite huge. (I fill a 128K part)

But if CW6 removes the file limitations, I wonder if it's time to consider an upgrade across the board for both my HC08 and 9S12 projects?

Anyone have any thoughts on this?

Mike
0 件の賞賛
返信

3,139件の閲覧回数
stanish
NXP Employee
NXP Employee
You can upgrade your previous CodeWarrior Special Edition license files.
Simply append "Win32_CWIDE_Unlimited" feature extracted from
CW HC08 v6.0 SE license to your license.dat file:

FEATURE Win32_CWIDE_Unlimited metrowks 5.9 permanent
   uncounted 8AEDAEE5CC12 VENDOR_STRING="CodeWarrior IDE 4.2 or
 
later, Windows" HOSTID=ANY ck=190

Then restart the CodeWarrior and 32 files per project limitation should be removed.


--
Alban Edit: correction wrapping


Message Edited by Alban on 2007-09-15 09:01 PM
0 件の賞賛
返信