FRDM-KL25Z as mouse

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,066件の閲覧回数
aayushm
Fresh Out Contributor

Has anyone worked on frdm-kl25z as air mouse in code warrior ? I'm facing problem with cursor movement. I need help as so as possible, I'm short of time.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
2,273件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

yes :-).

There are two things needed: accelerometer (Tutorial: Accelerating the KL25Z Freedom Board | MCU on Eclipse) and HID mouse (Using the FRDM-KL25Z as a USB Mouse Device | MCU on Eclipse). The resulting code with using X/Y axis for cursor movement is on GitHub (mcuoneclipse/Examples/FRDM-KL25Z/Freedom_USB_HID_Mouse/Sources/Application.c at master · ErichStyger...).

I hope this helps,

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,273件の閲覧回数
aayushm
Fresh Out Contributor

hi BlackNight

Thank you for the great contribution. I have been following your site and it had helped me a lot in learning kl25z.

The code works good :smileywink:

0 件の賞賛
返信
2,274件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

yes :-).

There are two things needed: accelerometer (Tutorial: Accelerating the KL25Z Freedom Board | MCU on Eclipse) and HID mouse (Using the FRDM-KL25Z as a USB Mouse Device | MCU on Eclipse). The resulting code with using X/Y axis for cursor movement is on GitHub (mcuoneclipse/Examples/FRDM-KL25Z/Freedom_USB_HID_Mouse/Sources/Application.c at master · ErichStyger...).

I hope this helps,

Erich

0 件の賞賛
返信