F800 in the lst file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

F800 in the lst file

1,980 Views
csosza
Contributor I

Hi,

 

Is it possible to generate the lst file with real addresses? The addresses in my lst file begin with

0000, however the simulator show, it is starting at F800 (register PC).

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,216 Views
CompilerGuru
NXP Employee
NXP Employee

Disassemble the elf file.

 

Daniel

1,216 Views
kef
Specialist I
Wow, nice feature, Daniel. However, *.abs file can't be opened in IDE. Abs file can be added to project files, then disassembled. And to be able to build project again (duplicated symbols in *.abs and *.o), do we need to remove abs file from project?