Errors when compiling project imported from BeeKit

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Errors when compiling project imported from BeeKit

跳至解决方案
1,884 次查看
karl_fsk
Contributor I
Hi, I am trying to use BeeKit(v 1.1.1.0) to generate a project and then import it into CodeWarrior (v5.7.0) according to AN3231(v1.1). However, when I compile the file using codewarrior, a lot of errors were reported. It seems the compilier can't find many header files. Why does this happen?
 
Thanks.
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
891 次查看
CrasyCat
Specialist III
Hello
 
You have to add the paths to the directory where the include files are located to the AccessPaths Panel.
Just open the target settings dialog (ALT + F7) and switch to Access Paths panel.
Then add the paths to your include files..
 
CrasyCat

在原帖中查看解决方案

0 项奖励
回复
1 回复
892 次查看
CrasyCat
Specialist III
Hello
 
You have to add the paths to the directory where the include files are located to the AccessPaths Panel.
Just open the target settings dialog (ALT + F7) and switch to Access Paths panel.
Then add the paths to your include files..
 
CrasyCat
0 项奖励
回复