Errors when compiling project imported from BeeKit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Errors when compiling project imported from BeeKit

ソリューションへジャンプ
2,275件の閲覧回数
karl_fsk
Contributor I
Hi, I am trying to use BeeKit(v 1.1.1.0) to generate a project and then import it into CodeWarrior (v5.7.0) according to AN3231(v1.1). However, when I compile the file using codewarrior, a lot of errors were reported. It seems the compilier can't find many header files. Why does this happen?
 
Thanks.
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,282件の閲覧回数
CrasyCat
Specialist III
Hello
 
You have to add the paths to the directory where the include files are located to the AccessPaths Panel.
Just open the target settings dialog (ALT + F7) and switch to Access Paths panel.
Then add the paths to your include files..
 
CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,283件の閲覧回数
CrasyCat
Specialist III
Hello
 
You have to add the paths to the directory where the include files are located to the AccessPaths Panel.
Just open the target settings dialog (ALT + F7) and switch to Access Paths panel.
Then add the paths to your include files..
 
CrasyCat
0 件の賞賛
返信