Error starting external debugger (Error Code 87), Vista, CW 4.6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error starting external debugger (Error Code 87), Vista, CW 4.6

ソリューションへジャンプ
3,746件の閲覧回数
ernestsnaith
Contributor I
I am trying to use a DEMO9S12XDT512 with CW on a Vista laptop. I have installed the latest special edition version and CW12_V4_6_HCS12X_USB_MULTILINK_SP. I still get Error starting external debugger (Error Code 87). Am I missing something, or is this another Vista issue?
 
Cheers
 
CodeWarrior IDE version 5.7.0
Build 2211
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,744件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
0 件の賞賛
返信
1 返信
1,745件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
I'm afraid that the latest HC12 version is not that recent.

See:
http://forums.freescale.com/freescale/board/message?board.id=CW816COMM&message.id=3280&query.id=1058...

Daniel

0 件の賞賛
返信