Error starting external debugger (Error Code 87), Vista, CW 4.6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error starting external debugger (Error Code 87), Vista, CW 4.6

Jump to solution
3,667 Views
ernestsnaith
Contributor I
I am trying to use a DEMO9S12XDT512 with CW on a Vista laptop. I have installed the latest special edition version and CW12_V4_6_HCS12X_USB_MULTILINK_SP. I still get Error starting external debugger (Error Code 87). Am I missing something, or is this another Vista issue?
 
Cheers
 
CodeWarrior IDE version 5.7.0
Build 2211
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,665 Views
CompilerGuru
NXP Employee
NXP Employee
0 Kudos
Reply
1 Reply
1,666 Views
CompilerGuru
NXP Employee
NXP Employee
I'm afraid that the latest HC12 version is not that recent.

See:
http://forums.freescale.com/freescale/board/message?board.id=CW816COMM&message.id=3280&query.id=1058...

Daniel

0 Kudos
Reply