Error import file default.cww

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error import file default.cww

ソリューションへジャンプ
1,807件の閲覧回数
Dekabrist
Contributor I

when I start CodeWarrior for DSC56800E v8.2.3 I see 8 messages about import error file default.cww, for example:

 

Error importing XML file "default.cww" near line 135.

Foung tag "DEBUGCONTEXT", which is invalid in this context.

 

Is this critical error for working CW?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,069件の閲覧回数
CrasyCat
Specialist III

Hello

 

This just prevents the IDE from loading the previous .mcp file when it is started.

If you open the .mcp file manually you should be safe.

 

In order to remove that issue you can try the following:

  - Close CodeWarrior

  - Open a Windows Explorer

  - Browse to %USERPROFILE%\Local Settings\Application Data\Metrowerks

  - delete the file default.cww located there

  - Start CodeWarrior again. You should not see that message any more.

 

CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,070件の閲覧回数
CrasyCat
Specialist III

Hello

 

This just prevents the IDE from loading the previous .mcp file when it is started.

If you open the .mcp file manually you should be safe.

 

In order to remove that issue you can try the following:

  - Close CodeWarrior

  - Open a Windows Explorer

  - Browse to %USERPROFILE%\Local Settings\Application Data\Metrowerks

  - delete the file default.cww located there

  - Start CodeWarrior again. You should not see that message any more.

 

CrasyCat

0 件の賞賛
返信