Error import file default.cww

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Error import file default.cww

跳至解决方案
1,811 次查看
Dekabrist
Contributor I

when I start CodeWarrior for DSC56800E v8.2.3 I see 8 messages about import error file default.cww, for example:

 

Error importing XML file "default.cww" near line 135.

Foung tag "DEBUGCONTEXT", which is invalid in this context.

 

Is this critical error for working CW?

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,073 次查看
CrasyCat
Specialist III

Hello

 

This just prevents the IDE from loading the previous .mcp file when it is started.

If you open the .mcp file manually you should be safe.

 

In order to remove that issue you can try the following:

  - Close CodeWarrior

  - Open a Windows Explorer

  - Browse to %USERPROFILE%\Local Settings\Application Data\Metrowerks

  - delete the file default.cww located there

  - Start CodeWarrior again. You should not see that message any more.

 

CrasyCat

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,074 次查看
CrasyCat
Specialist III

Hello

 

This just prevents the IDE from loading the previous .mcp file when it is started.

If you open the .mcp file manually you should be safe.

 

In order to remove that issue you can try the following:

  - Close CodeWarrior

  - Open a Windows Explorer

  - Browse to %USERPROFILE%\Local Settings\Application Data\Metrowerks

  - delete the file default.cww located there

  - Start CodeWarrior again. You should not see that message any more.

 

CrasyCat

0 项奖励
回复