Error:  Initialization Failed.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error:  Initialization Failed.

2,745 Views
arunkumar_it
Contributor I

Code warrior development studio professional edition V 8.8

=== Target Configuration Settings

=== Connection:   CodeWarrior USB TAP

=== Target Processor: 8349

Any idea to resolve this error?

 

Labels (1)
0 Kudos
Reply
4 Replies

2,398 Views
TICS_Fiona
NXP Employee
NXP Employee

It seems that the memory controller is not properly configured. Have you checked the memory operation with the help of the CodeWarrior Hardware Diagnostics applet?

0 Kudos
Reply

2,398 Views
trytohelp
NXP Employee
NXP Employee

Hi,

With the Project Wizard you can create an example for the processor and connection you're using.

this project will contain all default configuration needed.

You should be able to build it and debug the example application.

Is it working on your side ?

Regards

Pascal

0 Kudos
Reply

2,398 Views
arunkumar_it
Contributor I

Hi Pascal,

I have created the project with the required configuration, when i try to program the processor with the  load, it shows

Initialization failed error.

Thanks and Regards,

Arun

0 Kudos
Reply

2,398 Views
trytohelp
NXP Employee
NXP Employee

Another point ...

There are seveal patches for CW for PA V8.8.

You can access them via the link:

      http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-POWER-NETWORKING&fpsp=1&tab=Design...
expand the Updates and Patches (13)Expand All 

The last path is PA V8.8.6 which require another patch V8.8.5.

Pascal

0 Kudos
Reply