Eclipse device support question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Eclipse device support question

ソリューションへジャンプ
1,968件の閲覧回数
Ingo_Michael
Contributor II

Hello @ all!

 

I write all of my programms in assembly language using CW. Well, I bought a TWR-S08PT60 and CW does not support this device.

I think it would be time to switch to the new Eclipse IDE. But I am not sure if Eclipse support the S08PT60 device. I looked arround at the freescale

Webpage and found this link to Eclipse IDE and seen that S08PT is supported but it differs to the description in the brochure on page 7. On page 7 is a device list with all supportet devices.

 

What is correct? Can anyone check this for me? I would like to know if the S08PT is supported in Eclipse IDE using assembly language.

 

Please help if it is possible.

 

Have a good day,

 

Ingo

ラベル(1)
0 件の賞賛
返信
1 解決策
1,804件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

I'm using Eclipse based CodeWarrior for MCU10.3 beta (see CodeWarrior for MCU10.3 beta is now available | MCU on Eclipse) with my S08PT and that works fine.

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,805件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

I'm using Eclipse based CodeWarrior for MCU10.3 beta (see CodeWarrior for MCU10.3 beta is now available | MCU on Eclipse) with my S08PT and that works fine.

Erich

0 件の賞賛
返信
1,804件の閲覧回数
Ingo_Michael
Contributor II

Hello Erich!

Thank you very much! That was a very useful answer!

I have installed the beta version and it is working fine.

Thank you again!

BR Ingo

0 件の賞賛
返信