Drive a 7-segment LED directly from a S08P MCU

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Drive a 7-segment LED directly from a S08P MCU

跳至解决方案
1,114 次查看
juliancox
Contributor V

I am new to Codewarrior . Due to their demise I need to migrate a number of designs from LPC9XX devices to, in one case, a S08P4 (20-pin). I need to to drive a 7-segment LED directly from a S08P MCU, but the ports are not wide enough. Is there a way of "creating" a 7-bit wide port? Before anyone suggests it, I cannot use a larger device or peripheral hardware.

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
928 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

I am not sure that I got properly your question.

You need a 7 bit (7 pins) port on the soic 20 S08PA device? if this is the case you have available the complete port B 

the port B is on pins 5, 6 ,7 8 and 13 to 20.

Regards

Vicente Gomez

在原帖中查看解决方案

1 回复
929 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

I am not sure that I got properly your question.

You need a 7 bit (7 pins) port on the soic 20 S08PA device? if this is the case you have available the complete port B 

the port B is on pins 5, 6 ,7 8 and 13 to 20.

Regards

Vicente Gomez