[Discovery Options] page in project properties C/C++ Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[Discovery Options] page in project properties C/C++ Problem

1,418 Views
georglerm
Contributor I

Hi

 

I created a 'bareboard' C++ project for the FRDM-KL25Z  board.

I built the project with no errors, but when I start the debugger i get the '[Discovery Options] page in project properties C/C++ Problem' warning, and the process stops and prompts to continue with error or stop.

 

I had a look at the Discovery Options in the properties page, but this is a bit new to me, so not sure how to resolve this. When I ignore the error and continue to debugging it starts up everything and loads the code to the board and runs with no problem.

 

I have included a zip file with the project with this post. No modifications or any changes were made to the file or settings.

 

Any help/direction will be most appreciated.

 

Georg

Original Attachment has been moved to: testcpp1.zip

Labels (1)
Tags (2)
0 Kudos
Reply
2 Replies

1,105 Views
TICS_Fiona
NXP Employee
NXP Employee

What's the CodeWarrior version you are using? 1)Start the IDE and click on Help | About CodeWarrior Development Studio. 2)Provide us the info displayed.

0 Kudos
Reply

1,105 Views
georglerm
Contributor I

Apologies, should have included that.

Georg

I4852_4852.png

0 Kudos
Reply