Differences between version 6.2 and 6.3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Differences between version 6.2 and 6.3

ソリューションへジャンプ
2,486件の閲覧回数
Richard777
Contributor I

Hi guys, what are the differences between these two versions ?

 

Best regards

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,345件の閲覧回数
J2MEJediMaster
Specialist I

I was going to tell you that such information ought to be present on the CodeWarrior Downloads page, but it is not. I will look into that, but for the sake of getting your question answered, here is what the Welcome_CW_MCUs.txt file has on the subject:

 

This file contains information about the CodeWarrior Development Studio for Microcontrollers V6.3:

This release provides support for:
---------------------------------

(1) Newly supported derivatives:

      MC9RS08KB12, MC9RS08KB2, MC9RS08KB4, MC9RS08KB8, MC9RS08LA8, MC9RS08LE4,
      MC9S08FL16, MC9S08FL8, SC9S08IA2, SC9S08IA4, SC9S08IB4, SC9S08IB8, SC9S08IC8,
      MC9S08JS16, MC9S08JS16L, MC9S08JS8, MC9S08JS8L, MC9S08LG16, MC9S08LG32,
      MC9S08LL8, MC9S08LL16, MC9S08LL36, MC9S08LL64, MC9S08MP12, MC9S08MP16,
      MC9S08QB4, MC9S08QB8, MC9S08SC4, MC9S08SE4, MC9S08SE8, MC9S08SV16, MC9S08SV8,
      MCF51EM128, MCF51EM256, MCF51JM32, MCF51CN128

(2) Improved version of ColdFire V1 compiler

(3) Evaluation license provided for 30 days evaluation period.

(4) Updated P&E Support.

(5) Support for the new Freescale Open Source BDM connection based on HCS08JM60
  platform. The "HCS08 FSL Open Source BDM" and "CFV1 FSL Open Source BDM"    
  connections can   be selected in New Project Wizard for the new derivatives
  listed above.

(6) Debugger support for external memory debugging with MCF51CN128.

(7) Updated Processor Expert 3.07 Release

(8) New CodeWarrior Examples are provided.



 
********************************************************

LIMITATIONS:
----------- 

WINDOWS VISTA SPECIFIC LIMITATIONS:
-----------------------------------

The following limitations are applicable only if you are installing the product on Windows Vista:

(1) During installation, security messages may pop up concerning drivers being installed. It is highly
    recommended to click on the option "continue anyway..", so the drivers can be installed.

(2) When opening the Codewarrior components (IDE, Debugger etc.) Firewall warnings may appear
    with the option to block or unblock the application. It is advisable to click on the unblock option to
    continue.

(3) For more VISTA specific limitations after the installation, please refer to:
         "{INSTALLATION DIRECTORY}\Release_Notes\HC08\Notes_CW_MCUs_V6 3_Vista.txt"


GENERAL LIMITATIONS:
--------------------

The following limitations are applicable to Windows Vista, Windows XP:

(1) It is highly recommended to have at least 400 MB of free space on the Windows system disk.
(2) Product supports 32-bit versions of Windows XP, Windows Vista.
 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,346件の閲覧回数
J2MEJediMaster
Specialist I

I was going to tell you that such information ought to be present on the CodeWarrior Downloads page, but it is not. I will look into that, but for the sake of getting your question answered, here is what the Welcome_CW_MCUs.txt file has on the subject:

 

This file contains information about the CodeWarrior Development Studio for Microcontrollers V6.3:

This release provides support for:
---------------------------------

(1) Newly supported derivatives:

      MC9RS08KB12, MC9RS08KB2, MC9RS08KB4, MC9RS08KB8, MC9RS08LA8, MC9RS08LE4,
      MC9S08FL16, MC9S08FL8, SC9S08IA2, SC9S08IA4, SC9S08IB4, SC9S08IB8, SC9S08IC8,
      MC9S08JS16, MC9S08JS16L, MC9S08JS8, MC9S08JS8L, MC9S08LG16, MC9S08LG32,
      MC9S08LL8, MC9S08LL16, MC9S08LL36, MC9S08LL64, MC9S08MP12, MC9S08MP16,
      MC9S08QB4, MC9S08QB8, MC9S08SC4, MC9S08SE4, MC9S08SE8, MC9S08SV16, MC9S08SV8,
      MCF51EM128, MCF51EM256, MCF51JM32, MCF51CN128

(2) Improved version of ColdFire V1 compiler

(3) Evaluation license provided for 30 days evaluation period.

(4) Updated P&E Support.

(5) Support for the new Freescale Open Source BDM connection based on HCS08JM60
  platform. The "HCS08 FSL Open Source BDM" and "CFV1 FSL Open Source BDM"    
  connections can   be selected in New Project Wizard for the new derivatives
  listed above.

(6) Debugger support for external memory debugging with MCF51CN128.

(7) Updated Processor Expert 3.07 Release

(8) New CodeWarrior Examples are provided.



 
********************************************************

LIMITATIONS:
----------- 

WINDOWS VISTA SPECIFIC LIMITATIONS:
-----------------------------------

The following limitations are applicable only if you are installing the product on Windows Vista:

(1) During installation, security messages may pop up concerning drivers being installed. It is highly
    recommended to click on the option "continue anyway..", so the drivers can be installed.

(2) When opening the Codewarrior components (IDE, Debugger etc.) Firewall warnings may appear
    with the option to block or unblock the application. It is advisable to click on the unblock option to
    continue.

(3) For more VISTA specific limitations after the installation, please refer to:
         "{INSTALLATION DIRECTORY}\Release_Notes\HC08\Notes_CW_MCUs_V6 3_Vista.txt"


GENERAL LIMITATIONS:
--------------------

The following limitations are applicable to Windows Vista, Windows XP:

(1) It is highly recommended to have at least 400 MB of free space on the Windows system disk.
(2) Product supports 32-bit versions of Windows XP, Windows Vista.
 

0 件の賞賛
返信
1,345件の閲覧回数
Richard777
Contributor I

Thanks very much Jedi Master !!!

 

 

0 件の賞賛
返信