It would be GREAT if the debugger could show the internal timing based on the settings of the processor. Every time we set up a new processor we are forever trying to calculate baud rates, timers rates, input capture compare rates, overflow times etc Why doesnt it just show all this in the debugger 
Internal Clock =
Timer X singe clock time =
Baud rate =
ADC Conversion time =
Input/Output Capture singe clock time =
et
All the things the debugger can easily tell you...
If you could set an external xtal setting using some #pragma this would allow the debugger to tell you the same info when the external xtal is setup.
We have been moving a heap of designs from 05 to S08 and there are so many variation and changes its always a 'task' that should really be done for you...
I think beans look after this, but we just use straight c or assembly.
Message Edited by CarlFST60L on 2009-08-26 05:05 AM