Debug Error message

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Debug Error message

2,892 次查看
DMR_Embedded
Contributor I

Hi,

 

I am trying to create build, debug environment for MC9S12G128 - Memory model (Small). Just created and when t rying to flash with Debug tool, always getting error @FF80.

 

Please suggest.

标签 (1)
标记 (1)
0 项奖励
回复
4 回复数

2,623 次查看
Lundin
Senior Contributor IV

Seems strange that it attempts to download 512 bytes to that address. 512 happens to be the flash erase segment size on the S12, so that seems related to the issue. What does the vector table implementation look like and what does your .prm file look like?

 

If you are using some function pointer table implementation, you may have to declare the pointers as "near". Here is a better implementation in pure ISO C:

https://community.freescale.com/message/59586#59586

 

Also... did you try to unsecure the MCU just in case?

 

0 项奖励
回复

2,623 次查看
DMR_Embedded
Contributor I

 

You point on unsecuring is giving some catch.....

 

After unsecuring successfully, when we try to flash *. abs file, it fails

-----------------------------------------

FP:  No Programming voltage

-----------------------------------------

 

This is actually after executing VPPON command. Please help with your suggestions.

0 项奖励
回复

2,623 次查看
kef
Specialist I

There's no memory at 0x10000. I guess you used #pragma DATA_SEG <vectors_segment> directive to put vectors table somewhere at 0xFFxx. Vectors table should end at 0xFFFF. Below your table you should add #pragma DATA_SEG defualt to restore default constants placement. If you didn't do this and added some constants or strings below vectors table, then linker probably went above 0xFFFF and debugger is unable to flash that to nonexisting flash locations.

 

0 项奖励
回复

2,623 次查看
DMR_Embedded
Contributor I

Hi,

 

Actually there is no code after the address 0xFFFF, pls find the last few lines of the generated map file.

 

     main                                      C006       5       5          1   .text      
     MCU_init                               C00B      2C      44       1   .text      
     MCU_init_reset                    C037      12      18       3   NON_BANKED 
     isr_default                             C049       1       1         61   NON_BANKED 
     _InterruptVectorTable          FF80      7A     122       0   .abs_section_ff80
     _ResetVectorTable              FFFA       6       6         0   .abs_section_fffa

 

i am getting error while downloading application to debugger. Any other information could also be helpful.

0 项奖励
回复