Data reception from the slave through uart of MPC5746R

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Data reception from the slave through uart of MPC5746R

1,175 次查看
sujendra_n2
Contributor I

Hi,

I am using MPC5746R which is capable of 4 bytes data TX & data RX and i am having the requirement of receiving data of more than 5 bytes from the slave at 250kbaud.

Now i am trying to read byte by byte by checking status register and clearing it .

But i am not able to receive the data do we need to go for DMA in this case.

Please suggest me.

Thanks and Regards

N sujendra

标记 (1)
0 项奖励
回复
2 回复数

1,078 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

could you please STOP to create duplicated question? This question is solved by our engineer in Salesforce, so, please do not waste our resources.

Regards,

Martin

0 项奖励
回复

1,078 次查看
sujendra_n2
Contributor I

Dear Martin,

Actually we are not getting proper solution for that issue and one of your application engineer lukas helping us but he is also little busy till monday.

I have seen one post from you regarding FLEXCAN Interrupt of MPC5746R same way I tried it for uart for core zero but its not successful .

So I posted it to get example code for uart interrupt.

I have got example code from lukas today I will debug through it.

Thanks for your kind suggestion and inputs

Thanks and Regards

N sujendra

0 项奖励
回复