DWARF/ELF no debug information message - code will not simulate?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DWARF/ELF no debug information message - code will not simulate?

ソリューションへジャンプ
3,295件の閲覧回数
FC
Contributor III
Hi,
 
I am in the process to port the NEMOS embedded os demo to the HCS08QG8.  Here is the NEMOS os website: http://http://www.btielectronics.com/NEMOS.htm
 
I have modified the port to compile and to run on the DEMO9S08QG8 board.  I have not downloaded it yet.  However,  compiler gives the warning message of no debug info for the NEMOS_DEMO.c.o.
 
They provide the object file only.
 
Basically, I get no tasks to run.  Is it because the simulator cannot run the code?
 
Has anyone used NEMOS?  
 
Has anyone ported the HC08 uC/OS-II to the HCS08?
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,739件の閲覧回数
Lundin
Senior Contributor IV
In the project window, there is a column with a green 'bug' on it. For every linkable file in the project, click on this column.

I'm pretty sure this question should be in a FAQ somewhere.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,740件の閲覧回数
Lundin
Senior Contributor IV
In the project window, there is a column with a green 'bug' on it. For every linkable file in the project, click on this column.

I'm pretty sure this question should be in a FAQ somewhere.
0 件の賞賛
返信
1,739件の閲覧回数
UK_CF_FAE
NXP Employee
NXP Employee
You can do the same thing by clicking on the source file, then opening the Project Inspector, going to the 2nd tab (if I remember) and selecting Debug Info....