DEVKIT-S12ZVC peripheral Library CodeWarrior

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DEVKIT-S12ZVC peripheral Library CodeWarrior

3,410 Views
christinar
Contributor II

Hi,

at first sorry for my english. I´m a student from germany and this is my first project with a microcontroller.

I´m using a DEVKIT-S12ZVC Board (9S12ZVCA192 microcontroller). There is only a #include for "peripheral declarations" in CodeWarrior. Is there a library containing ready functions which can be used for example setting the registers? Normally you have to implement a code like this on yourself:

void ADC_init(void){

ADC0CTL_0 = 0x0D; /*Dual Access mode and trigger mode selected */

ADC0CTL_1 = 0x00; /* Single command and result value list */

ADC0TIM = 0x0F; /*No prescaler selected */\

ADC0FMT = 0x82; /* Left justified and 10 bit resolution */

/* ADC0 Command & Result Base Pointers */

ADC0CBP_0 = (unsigned char)(((long)adc0_cmdlist) >> 16);

ADC0CBP_1 = (unsigned char)(((long)adc0_cmdlist) >> 8);

ADC0CBP_2 = (unsigned char)((long)adc0_cmdlist);

// ADC0 Result Base Pointer

ADC0RBP_0 = (unsigned char)(((long)adc0_results) >> 16);

ADC0RBP_1 = (unsigned char)(((long)adc0_results) >> 8);

ADC0RBP_2 = (unsigned char)((long)adc0_results);

ADC0CTL_0_ADC_EN= 1; /*Enables the ADC */

}

unsigned int ADC_read(unsigned int channel){

adc0_cmdlist[0][1] = 0xC0|channel;

ADC0FLWCTL_RSTA = 1; // Restart Event

while(0x00 == ADC0CONIF){} //wait until conversion is complete

ADC0CONIF = ADC0CONIF;//clear flag

return adc0_results[0];

}

 

unsigned int ADC_read_PGA(unsigned int channel, unsigned char PGA_in){

adc0_cmdlist[0][0] = 0xC0|(PGA_in<<4);

adc0_cmdlist[0][1] = 0xC0|channel;

ADC0FLWCTL_RSTA = 1; // Restart Event

while(0x00 == ADC0CONIF){} //wait until conversion is complete

ADC0CONIF = ADC0CONIF;//clear flag

return adc0_results[0];

}

Can I download or add a library which includes standards like the example?

Thank you in advane.

Kind regards

Christina

Labels (1)
0 Kudos
Reply
7 Replies

3,008 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Christina,

Processor expert can support S12Z project. we can use processor expert to generate peripheral initialization code.

Attached is the video shows how to create a processor expert project. Hope it helps.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,008 Views
christinar
Contributor II

Hi Jennie,

thank you for the information.

It´s my first time working with microcontrollers. I started with the "DEVKIT-S12ZVC-LAB" Examples but I can´t find descriptions for the Examples?

Do you know if there is a description?

Thank you in advance

Have a nice day,

Christina

0 Kudos
Reply

3,008 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

I haven't find any document describing this LAB. But I check the LAB  source comments which are very detail. 

I think you can refer the code comments to understand the code.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,008 Views
christinar
Contributor II

Yes the comments in the code are very helpful but I want to test the funktion of the code/board. Do I need two boards which are connected? (If yes, is it the same for testing CAN?)

In the description of DEVKIT-S12XE is an example for I2C/CAN. Maybe it´s similar to the S12ZVC board?

Description LAB3 and LAB4 DEVKIT-S12XE:

pastedImage_1.png

pastedImage_2.png

Thank you in advance.

Kind regards 

Christina

0 Kudos
Reply

3,008 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Yes, You'd better have two boards to test the communication.

Jennie Zhang

0 Kudos
Reply

3,008 Views
christinar
Contributor II

Ok thank you very much.

Kind regards

Christina

0 Kudos
Reply

3,008 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome!


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply