Custom printf handler for CW MCU 10.2/Kinetis

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Custom printf handler for CW MCU 10.2/Kinetis

1,442件の閲覧回数
konrada
Contributor IV

Hello everyone,

 

our C++ project targets CW10.2 on Kinetis and uses EWL. We've written our own custom logger. Now, a third-party library thinks it may just call printf() to output error messages. Currently, the EWL printf writes these messages to the debugger via some kind of Cortex debug magic.

 

Instead, I'd like to redirect the output to our logger. I've tried defining my own __ConsoleWrite function in my application, but that changed nothing; the printf call still went to the debugger. What else can I try? I'd like to keep the other C standard library functions, so I'd like to continue including EWL.

 

Greetings

KA 

ラベル(1)
0 件の賞賛
返信
1 返信

1,145件の閲覧回数
PetrC
Contributor II

Hi

Not sure about the C++ project, but in C project I use to define functions with the following prototypes to redirect printf:

int __read_console(__file_handle handle, unsigned char* buffer, size_t * count);
int __write_console(__file_handle handle, unsigned char* buffer, size_t* count);
int __close_console(__file_handle handle);

 

Regards

PetrC