Custom 9s12 board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Custom 9s12 board

2,336 Views
Mway
Contributor I

Hi I’ve made a custom development board with 9s12dt128 have all the connections and bdm working working however it seems my mcu is not operating as I upload code and doesn’t seem to work. I have a clock signal at eclk pin I am running with mhz external crystal and believe everything is connected correctly

 

0 Kudos
Reply
3 Replies

2,304 Views
Mway
Contributor I

How do you calculate resistor values and capacitor values for pll circuit I’m using 8mhz crystal pierce setup it seems the clock and bus clock is very unstable

0 Kudos
Reply

2,295 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI Mway 

If you wonder the problem is caused by hardware design, I suggest you check with 16bit MCU space rather than CW space:

https://community.nxp.com/t5/S12-MagniV-Microcontrollers/bd-p/16-bit

Have a nice day

Jun Zhang

0 Kudos
Reply

2,320 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

Could you please confirm if you can download project to the target successfully: Create a new project with wizard, after download the code, can you step over the code in debugger?

Please record me a video about the download and step over in debugger. I will check if there is any problem.

Thanks,

Jun Zhang 

0 Kudos
Reply