Crashing Flash programmer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Crashing Flash programmer

1,256 Views
jlange
Contributor I

I tried to flash my MPC5604P via CW 10.7.

So i open the Flash programmer and create a new Connection. When it comes to selecting the Connection type i can choose between "GDI Generic" and "P&E Power PC Multilink\Multilink Universal\Cyclone Max\OSJTAG". I need the second one.

After i choose it, CW will load for some seconds until it finally Chrashes. It will not Crash when i choose GDI Generic.

unfortunately i can't find any error log to look further into the problem.

Any idea whats wrong there?

Ps.:

I use Windows 10 Pro 64 Bit

Regards, Jan

Tags (2)
0 Kudos
Reply
0 Replies