Compiler syntax error for NXP files??

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Compiler syntax error for NXP files??

3,185 Views
pgillaspy
Contributor III

Below is the compiler errors encountered while compiling my program on CodeWarrior V11.1 with DSC QuickStart 2.7.3 for the 56F83789 processor.  The syntax error report is completely meaningless to me. This error is reported for virtually every freemaster.* source file. Please help interpret.

C:/Freescale/CW MCU v11.1/MCU/DSP56800x_EABI_Tools/command_line_tools/mwcc56800e|Compiler|Error
(C:\Users\PhilG\Hummingbird\MCE\MCESimplex\Simplex\SystemConfig\56F83789_Build_FLASH_LDM_LPM_OSJTAG.launch|1|0|1|0|1)
=<?xml version="1.0" encoding="UTF-8" standalone="no"?>
>declaration syntax error
>(included from:
> (command-line defines):1
> (C-C++ Preprocessor Panel):1
>
>C:\NXP\DSC56800EX_Quick_Start_r2.7\src\support\freemaster\freemaster_56F8xxx.c
>:1)
C:/Freescale/CW MCU v11.1/MCU/DSP56800x_EABI_Tools/command_line_tools/mwcc56800e|Compiler|Error
(C:\Users\PhilG\Hummingbird\MCE\MCESimplex\Simplex\SystemConfig\56F83789_Build_FLASH_LDM_LPM_OSJTAG.launch|1|0|1|0|1)
=<?xml version="1.0" encoding="UTF-8" standalone="no"?>
>declaration syntax error
>(included from:
> (command-line defines):1
> (C-C++ Preprocessor Panel):1
>
>C:\NXP\DSC56800EX_Quick_Start_r2.7\src\support\freemaster\freemaster_appcmd.c:
>1)
C:/Freescale/CW MCU v11.1/MCU/DSP56800x_EABI_Tools/command_line_tools/mwcc56800e|Compiler|Error
(C:\Users\PhilG\Hummingbird\MCE\MCESimplex\Simplex\SystemConfig\56F83789_Build_FLASH_LDM_LPM_OSJTAG.launch|1|0|1|0|1)
=<?xml version="1.0" encoding="UTF-8" standalone="no"?>
>declaration syntax error
>(included from:
> (command-line defines):1
> (C-C++ Preprocessor Panel):1
>
>C:\NXP\DSC56800EX_Quick_Start_r2.7\src\support\freemaster\freemaster_can.c:1)
C:/Freescale/CW MCU v11.1/MCU/DSP56800x_EABI_Tools/command_line_tools/mwcc56800e|Compiler|Error
(C:\Users\PhilG\Hummingbird\MCE\MCESimplex\Simplex\SystemConfig\56F83789_Build_FLASH_LDM_LPM_OSJTAG.launch|1|0|1|0|1)
=<?xml version="1.0" encoding="UTF-8" standalone="no"?>
>declaration syntax error
>(included from:
> (command-line defines):1
> (C-C++ Preprocessor Panel):1
>
>C:\NXP\DSC56800EX_Quick_Start_r2.7\src\support\freemaster\freemaster_fastrec.c
>:1)

0 Kudos
Reply
4 Replies

3,167 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

If you create a project and generate code based QuickStart tools without Freemaster device, can you compile successfully?

From your description, it appears it is a compiler option problem.

If it is convenient, pls post your project to us so that we can have a test.

BTW, we have SDK package for MC56F83xxx, which is official code generating tools.

https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-s...

Hope it can help you

BR

XiangJun Rong

 

0 Kudos
Reply

3,163 Views
pgillaspy
Contributor III

What do I need to do to compile without Freemaster? Delete the support/freemaster directory? Exclude support/freemaster from build?  Can you explain what Freemaster is?

0 Kudos
Reply

3,158 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The Freemaster tools is a tools run on PC side which can display  variables in customer application via uart, Jtag, CAN or whatever interface while the application is running in LPC/Kinetis/i.mxrt... family. 

If you do not need it, you can delete all the file in Freemaster directory.

You can download Freemaster tools from the link:

https://www.nxp.com/design/software/development-software/freemaster-run-time-debugging-tool:FREEMAST...

 

Hope it can hep you

BR

XiangJun Rong

0 Kudos
Reply

3,068 Views
pgillaspy
Contributor III

I deleted Freemaster stuff. All is well.

0 Kudos
Reply