Compile C++ with g++ and C with gcc in CW10.6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Compile C++ with g++ and C with gcc in CW10.6

1,156 Views
johannesschock
Contributor II

Hello,

I'm currently porting a large Project from CW 10.4 (Freescale Toolchain) to CW 10.6 (GCC Toolchain).

Im currently facing the Problem with having both c++-files and c-files with g++.

But I want the c++-files compiled with the g++ and the c-files compiled with gcc.

Is there a solution?

Regards, Johannes Schock

Labels (1)
0 Kudos
Reply
1 Reply

946 Views
BlackNight
NXP Employee
NXP Employee
0 Kudos
Reply