Compile C++ with g++ and C with gcc in CW10.6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Compile C++ with g++ and C with gcc in CW10.6

1,151件の閲覧回数
johannesschock
Contributor II

Hello,

I'm currently porting a large Project from CW 10.4 (Freescale Toolchain) to CW 10.6 (GCC Toolchain).

Im currently facing the Problem with having both c++-files and c-files with g++.

But I want the c++-files compiled with the g++ and the c-files compiled with gcc.

Is there a solution?

Regards, Johannes Schock

ラベル(1)
0 件の賞賛
返信
1 返信

941件の閲覧回数
BlackNight
NXP Employee
NXP Employee
0 件の賞賛
返信