Compilation or not compilation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Compilation or not compilation

1,280件の閲覧回数
PhilFree
Contributor II

Hello,

 

I have found a little bug in codewarrior 10.4 :

Processor = MS9S08QE128

Project mixed with C and ASM, parts in separate sources (ASM not in C sources)

 

- Variable declared in C ex: char VAR1

 

ASM Include sources: asm_var.inc

content:

XREFB           VAR1

FOO:               EQU  5

 

Assembly source: asm_main.asm

content:

INCLUDE 'asm_var.inc'

 

label:

     MOV     FOO,VAR1

     RTS

 

Compilation build project = OK, no errors

 

The values in asm_var.inc are modified like this and saved on disk

XREFB           VAR12345

FOOZSQ:       EQU  5

 

Compilation build project = OK, no errors !!!

 

To find the errors, I need to clean the project and rebuild it. With "normal" compilation this big bug is not detected.

I try to rename the include file asm_var.inc  in  asm_var.s, coloring syntax appear but the bug remain.

 

With the same wrong value in include file and adding an error on keyword XREFB

XREFBx           VAR12345

FOOZSQ:       EQU  5

 

The error is now detected, it's seems that variables are not always verified by the builder ??


 

Thank you

Philippe

 

 


ラベル(1)
タグ(4)
0 件の賞賛
返信
1 返信

1,216件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

or in other words: the GNU make file is not properly tracking the assembly include file dependencies.

I faced that problem too and have filed a bug report on this.

I know that this does not help, but at least I can confirm the issue.

As a workaround, if you change a .inc file, either change/touch the assemly file(s) using it, or do a clean as you already did.

I hope this helps (at least somewhat).