Compare 2 dates

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Compare 2 dates

2,820件の閲覧回数
MSI_Souza
Contributor I

I need compare two different dates. How I do?

I am using CodeWarrior S12(X) V5.0

 

Thanks.

ラベル(1)
タグ(1)
0 件の賞賛
返信
4 返答(返信)

2,489件の閲覧回数
Monica
Senior Contributor III

Claudio, are these replies useful?

We would like to know how is your project moving along!

Regards!

0 件の賞賛
返信

2,489件の閲覧回数
CrasyCat
Specialist III

Hello

 

Are you looking for time management function inside of the ANSI library?

 

The delivered library do not provide support for time management functions.

If you intend to use these functions in your application you need a dedicated hardware to handle time functions.

 

Comparing two different dates depends on how the device is programmed.

 

 

CrasyCat

0 件の賞賛
返信

2,489件の閲覧回数
usmanjavaid
Contributor II

what if cladio souza saves those 2 dates in two variables and put a check on their difference

.

when difference is zero the dates are same

.

similarly difference might be greater or smaller than 0

0 件の賞賛
返信

2,488件の閲覧回数
usmanjavaid
Contributor II

what if cladio souza saves those 2 dates in two variables and put a check on their difference

.

when difference is zero the dates are same

.

similarly difference might be greater or smaller than 0

0 件の賞賛
返信