Combining strings in CodeWarrior for the MC68HC812

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Combining strings in CodeWarrior for the MC68HC812

3,480 Views
tomrussell
Contributor I

Hi,

 

I'm a student doing a microprocessors segment on my degree at Coventry University and we've been given an assignment for the above processor (exact # is MC68HC812A4) - you'll have to bear with me a bit because this is the first time i've done anything along these lines :smileyhappy:

 

We're producing a simple program in C++ and as part of it i'd like to do some string operations

 

i.e.

 

char item1[3] = "0x0";

char item2[1] = "F";

char result;

 

strcat(result,item1);

strcat(result,item2);

 

Led_Port=result;

 

I've attempted to #include <string.h> at the top of the file, but when i go into the true-time debugger and attempt to run this code segment, the debugger halts at the strcat operation and the 'code' window says 'STRING.C NOT FOUND'.

 

Can anyone help? I'm probably making some kind of schoolboy error - or rather student error!

 

Thanks in advance.

Labels (1)
Tags (1)
0 Kudos
Reply
5 Replies

1,579 Views
CompilerGuru
NXP Employee
NXP Employee

It appers that the program is much more in C than in C++.

Check the sized of your arrays (result should be an array too, I guess this is a copy paste bug).

The arrays have to be large enough to contain a terminating 0 byte too, item1 and item2 are both too small.

If you do not change a variable, its good practise (and important on a small device) to make the variable const.

And if a variable only contains a const string, its less error prone not to define the size of the array.

E.g. static const char item1[] = "0x0";

 

Also make sure that the destination buffer is setup when you do the first strcat.

 

Daniel

0 Kudos
Reply

1,579 Views
bigmac
Specialist III

Hello,

 

Further to Daniel's comments, it would appear that the result variable should be defined as either an array or a pointer.

 

Regards,

Mac

 

0 Kudos
Reply

1,579 Views
tomrussell
Contributor I
Sorry - i should also add that this occurs whenever i try and use any 'str' operation - i'm not in the lab at the moment and the c++ code up there is probably far from correct and wouldn't compile :smileyhappy:
0 Kudos
Reply

1,579 Views
J2MEJediMaster
Specialist I

It sounds like you're not including the appropriate library that would contain the string handling functions. Did you use the New Project wizard to make the project?

 

---Tom

Message Edited by J2MEJediMaster on 2009-02-24 09:35 AM
0 Kudos
Reply

1,579 Views
tomrussell
Contributor I

Yeah, i did - created a C++ only project. CodeWarrior shows me having the following files in the filetree:

 

Sources

-main.cpp

-datapage.c (?)

Startup Code

-Start12.cpp

Libraries

-mc68hc812a4.h

-mc68hc812a4.c

-ansisi.lib

-cppsi.lib

 

I thought including the #include <string.h> in the header would import it from another filestore on compile though?

 

0 Kudos
Reply