Hi,
I'm a student doing a microprocessors segment on my degree at Coventry University and we've been given an assignment for the above processor (exact # is MC68HC812A4) - you'll have to bear with me a bit because this is the first time i've done anything along these lines ![]()
We're producing a simple program in C++ and as part of it i'd like to do some string operations
i.e.
char item1[3] = "0x0";
char item2[1] = "F";
char result;
strcat(result,item1);
strcat(result,item2);
Led_Port=result;
I've attempted to #include <string.h> at the top of the file, but when i go into the true-time debugger and attempt to run this code segment, the debugger halts at the strcat operation and the 'code' window says 'STRING.C NOT FOUND'.
Can anyone help? I'm probably making some kind of schoolboy error - or rather student error!
Thanks in advance.
It appers that the program is much more in C than in C++.
Check the sized of your arrays (result should be an array too, I guess this is a copy paste bug).
The arrays have to be large enough to contain a terminating 0 byte too, item1 and item2 are both too small.
If you do not change a variable, its good practise (and important on a small device) to make the variable const.
And if a variable only contains a const string, its less error prone not to define the size of the array.
E.g. static const char item1[] = "0x0";
Also make sure that the destination buffer is setup when you do the first strcat.
Daniel
Hello,
Further to Daniel's comments, it would appear that the result variable should be defined as either an array or a pointer.
Regards,
Mac
It sounds like you're not including the appropriate library that would contain the string handling functions. Did you use the New Project wizard to make the project?
---Tom
Yeah, i did - created a C++ only project. CodeWarrior shows me having the following files in the filetree:
Sources
-main.cpp
-datapage.c (?)
Startup Code
-Start12.cpp
Libraries
-mc68hc812a4.h
-mc68hc812a4.c
-ansisi.lib
-cppsi.lib
I thought including the #include <string.h> in the header would import it from another filestore on compile though?