Codewarrior v6.3 uncompatible with win7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior v6.3 uncompatible with win7

1,378件の閲覧回数
550121598
Contributor I

I install Codewarrior v6.3,prompted bellows:

    Codewarrior Development studio for Microcontrollers v6.3 is not compatible with windows XP 64-bit installation;

How can I solve this problem?

0 件の賞賛
返信
1 返信

1,272件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

CW6.3 can't support win7 64bit.

If you use HCS08 MCU, please use CW11 instead which is for 64 bit platform:

CodeWarrior® for Microcontrollers-Eclipse IDE 11.1 | NXP 


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信