Codewarrior and Doxygen

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior and Doxygen

2,458件の閲覧回数
sebastianhernan
Contributor I

Hi everyone

i have a problem installing the app of doxygen(Doxygen is a compiler which generates documentation out of source files.)

After installing all of them, finally the Eclox Eclipse plugin: point Eclipse to the Ecloxupdate site:http://download.gna.org/eclox/update/86868_86868.pngerrores.png

86869_86869.pngerroer2.png

i have to dowload the app

87131_87131.pngerrores3.png

after to install all

i click in the app for doing documentation

87132_87132.pngerrores4.png

the doxygen ask me for a doxyfile name,

when i click  finish this error display

87133_87133.pngerrores6.png

this is my question which is the error?

i try to reinstall codewarrior and eclox app

any help would be good, thank you.

ラベル(1)
0 件の賞賛
返信
1 返信

1,750件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Sebastian,

I'm not sure what could be causing this problem but please take a look to the following post created by our colleague Erich Styger, as you can see in the comments Shenzhen had the same issue and fixed it by creating the Doxyfile with Doxywizard and copied the Doxywizard into the project:

5 Best Eclipse Plugins: #1 (Eclox with Doxygen, Graphviz and Mscgen) | MCU on Eclipse

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 件の賞賛
返信