Codewarrior Multilink Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior Multilink Error

ソリューションへジャンプ
2,753件の閲覧回数
admin
Specialist II

We are currently trying to program a XBee 868LP device using the PE Micro Multilink Interface REV C and CodeWarrior Development Studio. Both the lights on the multilink is on and the device appears in the device manager and in CodeWarrior. However, when we try to program a section of code we get the error message included in the attachments. We have tryed to reinstall the drivers for the Multilink, reinstall Codewarrior and we have even tryed 3 diffrent XBee devices.

 

Any ideas for how to fix this problem?

 

 

Thanks,

Ole K.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,464件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Kristian:

What is the procedure you are following to program the device?

Sometimes this errors are caused because of a wrong selection of the target MCU. Have you verified with the datasheet that the device is the same as in your project?

Regards!

Jorge Gonzalez

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,465件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Kristian:

What is the procedure you are following to program the device?

Sometimes this errors are caused because of a wrong selection of the target MCU. Have you verified with the datasheet that the device is the same as in your project?

Regards!

Jorge Gonzalez

0 件の賞賛
返信