Codewarrior Basic and Kinetis

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior Basic and Kinetis

2,980件の閲覧回数
Glogov_Kolac
Contributor II

I want to buy CW 10.1 Basic edition for Kinetis K60 developement on MQX RTOS. Is there are any restrictions in Basic edition which will afect my developement except RTOS awerness in debugging. Basic edition have 512K limit which is exact the maximum Flash for the K60 MCU !

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,743件の閲覧回数
J2MEJediMaster
Specialist I

Go to this Freescale CodeWarrior suite comparison page and select the Kinetis part from the list at the left. The table specifies what tool capabilities are available for a given CodeWarrior suite.

 

---Tom

2,743件の閲覧回数
Glogov_Kolac
Contributor II

It seems that Basic edition will be enough for  most Kinetis MCU (except 1MB devices). My question is if the code size and absence of RTOS awerness is the only lack in Basic edition comparing to CW Professional ?! 

0 件の賞賛
返信