Codewarrior 6.3 PEMicroProtocolPlugin: No USB Connection found

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior 6.3 PEMicroProtocolPlugin: No USB Connection found

1,565 Views
timfloto
Contributor I

Hi,

I am using CW6.3 legacy tool on Windows XP to compile a "Helloworld" program for MCF 5282 board. Code compiles, builds and I am able to create a .S19 file also. But if I try to connect MCF 5282 through PE Cyclone MAX remote debugger it fails saying "PEMicroProtocolPlugin: No USB connection found".

I tried for different speed on each USB port, but no luck.

Speed tried: 5, 15, 3 for USB0, USB1, USB2, USB3.

Device Manager is able to successfully detect the Jungo driver.

It's been 3 months trying to figure out how to run a sample MCF 5282 program through PE Cyclone MAX. Need urgent help please!!

pastedImage_1.png

0 Kudos
Reply
1 Reply

1,468 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Tim,

Have you tried installing the latest P&E drivers on your computer?


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 Kudos
Reply