Codewarrior 10.6 Simulator

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior 10.6 Simulator

3,175 Views
mayursavaj
Contributor III

Hi,

We are using CW10.6 for kinetics. 

How to Use Simulator in CW10.6???

Thanks,

Mayur

0 Kudos
Reply
3 Replies

2,548 Views
stanish
NXP Employee
NXP Employee

Hi,

I'm affraid there is no Simulator for S12Z available in CodeWarrior for MCUs.

As far as I know there is simulator available in Cosmic development environment for S12Z (https://www.cosmic-software.com/s12z_des.php)

Hope it helps.

Stan

0 Kudos
Reply

2,649 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

CW eclipse doesn't install simulator plugin for kinetis. There is no way to simulate chip run without connecting a board.

some 8bit and dsc chip has full chip simulator installed but not for kinetis.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,591 Views
manjunathkm
Contributor III

Can i use simulator for S12Z micro for the same IDE 10.6 version?

0 Kudos
Reply