Codewarrior 10.4 installing error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Codewarrior 10.4 installing error

跳至解决方案
3,440 次查看
mithunp_s
Contributor III

Dear All,

 

One of my customer is trying to Install Codewarrior in their system but they are getting attached error, if we please help to resolve.

 

Please let me know if this is because of system administrator Security error so that I can ask them to check with their administrator end, they are using windows XP.

 

Regards

Mithun

标签 (1)
0 项奖励
回复
1 解答
3,252 次查看
TICS_Fiona
NXP Employee
NXP Employee

You may trust CW, and continue the installation.

To reply your question about System Requirements:

1) Recommended Configuration

2.6GHz Pentium® compatible processor or better

4GB RAM

20GB (When installing full product or updates for all architectures)

400MB on Windows system disk

DVD drive for installation

USB port for communications with target hardware

Ethernet port for communications with target hardware (optional)

2) Operational Minimum Configuration

1.8GHz Pentium® compatible processor or better

2GB RAM

20GB (When installing full product or updates for all architectures)

400MB on Windows system disk

DVD drive for installation

USB port for communications with target hardware

3) Host Operating System Support

Microsoft® Windows XP 32-bit and 64-bit (Professional Edition)

Microsoft Windows 7 32-bit and 64-bit (Home Premium Edition and Professional Edition)

Windows 8 32-bit and 64-bit (Home Premium Edition and Professional Edition)

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,252 次查看
TICS_Fiona
NXP Employee
NXP Employee

It seems that this error prompts when installing USBTAP driver. Have you ever installed any other CodeWarrior tool on this PC? I think you can ignore this error, and go on installing, because even if the USBTAP driver is not installed successfully, we can install it separately later.

0 项奖励
回复
3,252 次查看
mithunp_s
Contributor III

Hi,

We have not installed any codewarrior earlier we are using this first time and trying to install CW10.4.

We have tried it on two more PC's but the same error is popping up, please help how to resolve the issue.

We are using windows XP, please let us know the minimum system requirement to get codewarrior running.

Regards

Mithun

0 项奖励
回复
3,253 次查看
TICS_Fiona
NXP Employee
NXP Employee

You may trust CW, and continue the installation.

To reply your question about System Requirements:

1) Recommended Configuration

2.6GHz Pentium® compatible processor or better

4GB RAM

20GB (When installing full product or updates for all architectures)

400MB on Windows system disk

DVD drive for installation

USB port for communications with target hardware

Ethernet port for communications with target hardware (optional)

2) Operational Minimum Configuration

1.8GHz Pentium® compatible processor or better

2GB RAM

20GB (When installing full product or updates for all architectures)

400MB on Windows system disk

DVD drive for installation

USB port for communications with target hardware

3) Host Operating System Support

Microsoft® Windows XP 32-bit and 64-bit (Professional Edition)

Microsoft Windows 7 32-bit and 64-bit (Home Premium Edition and Professional Edition)

Windows 8 32-bit and 64-bit (Home Premium Edition and Professional Edition)

0 项奖励
回复
3,252 次查看
mithunp_s
Contributor III

Thank you very Much for the details.

Regards

Mithun

0 项奖励
回复