Erich Styger schrieb:
There are no plans for 10.3 and Linux. Alternatives on Linux are CodeRed or Cocox.
So there is no chance anymore to code and debug HCS08 devices under linux with an up-to-date ide / toolchain?
Tassilo
Are you saying that Freescale has abandoned any and all tools that run on the Linux platform?!
CW10.2 is the LAST version for Linux?!
If this is the case, then WHAT is the reason for dropping Linux and where did this mandate come from?
I see. So in order to use Codewarrior 10.3 we will need to purchase a Microsoft license for Winxxx instead of using our Linux machines which worked just fine with Codewarrior 10.2.
If Freescale cannot support our platform of choice, then we will no longer support Freescale (i.e. no more Freescale designs.). Our company does not do Windows due to the security risks associated with that OS.