CodeWarrior under WIN-7 Virtual XP and real time debugging II

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior under WIN-7 Virtual XP and real time debugging II

Jump to solution
5,087 Views
mardalianis
Contributor III

I've installed CodeWarrior for Microcontrollers v6.3 under the Virtual XP running on a x64 i7 and Win-7. 

Initally I installed the BDM (USB) inteface driver (V10) under the Virtual XP. CodeWarrior could not talk to the BDM. It reports that the port is undetected. Clicking the Virtual XP "Device Manager" button, the Jungo Windriver is present but not the USB Multilink 2.0 (Rev. B, updated with the latest firmware).

After that, I installed the same driver also under Win 7. Nothing changed. The port was again undetected. Clicking the Windows7 "Device Manager" button, the Jungo Windriver and the USB Multilink 2.0 were both present.

Any suggestions to this problem? I personally think that Freescale should already have Codewarrior run under Win7.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
4,143 Views
mardalianis
Contributor III

Hi,

thank you both for your help.

I managed to install and run CW 6.3 under Win7, following the instructions on this topic:

https://community.freescale.com/message/68969#68969

Then I remembered I hade somewhere a Cyclone PRO. Since the same problem appeared connecting it on the USB port, I then used the Ethernet Interface (after updating it's firmware on an XP machine) and it works fine.However Multilink is easier to use. So kef I will try the solution you suggest and post the result.

Mardalianis

View solution in original post

0 Kudos
Reply
6 Replies
4,143 Views
kef
Specialist I

Mardalianis,

 

in WinXP Mode window, I think you should use USB drop down menu to Attach Multilink USB device to WinXP Mode Virtual Machine. By default USB devices other than flash disks are dedicated to Win7 host machine, so you need to click Attach to make device connected to virtual machine. I once managed to make Multilink working from WinXP mode window.

 

0 Kudos
Reply
4,144 Views
mardalianis
Contributor III

Hi,

thank you both for your help.

I managed to install and run CW 6.3 under Win7, following the instructions on this topic:

https://community.freescale.com/message/68969#68969

Then I remembered I hade somewhere a Cyclone PRO. Since the same problem appeared connecting it on the USB port, I then used the Ethernet Interface (after updating it's firmware on an XP machine) and it works fine.However Multilink is easier to use. So kef I will try the solution you suggest and post the result.

Mardalianis

0 Kudos
Reply
4,143 Views
mardalianis
Contributor III

It did not work. Under win7 the Multilink blue led lit then in win XP mode window after attaching it, the PC installed the driver again.Running CW I received the same message (port undetected). I restarted the XP mode and when I attached the Multilink again the blue led went off and I received a win7 message, that an unknown device was detected etc..

So, to the moment, I will work with CyclonPRO and the Ethernet connection and later on I will come back.

Mardalianis

 

0 Kudos
Reply
4,143 Views
Codewarriorunde
Contributor I

Hi,

I have a same problem. I installed a last PE usb driver under win-7 (pro version). When JTAG attached to the usb port

the LED is on, but when I attach to the usb under XP virtual machine I got a failure message.

What should I do? (I have no other type JTAG as Mardalianis)

Thanks.

Boris.

0 Kudos
Reply
4,143 Views
J2MEJediMaster
Specialist I

You might want to take a look at application note AN4338, which describes a workaround for the USB driver issue. While the technique described is unsupported by Freescale and pertains to CW for MobileGT and CW for DSCs, it might be worth a try.

 

Don't forget to download the software archive associated with this app note, which is located in the archive file AN4338SW.zip.

 

---Tom

0 Kudos
Reply
4,141 Views
J2MEJediMaster
Specialist I

 Take a look in this forum thread for some information on dealing with Win 7.

 

---Tom

0 Kudos
Reply